Safety and Flexibility in Deep Water - Trelleborg Fluid Handling Solutions - Trelleborg AB

Safety and Flexibility in Deep Water

Trelleborg’s Trelline® system is a cost-effective alternative for deepwater oil exploration.
Oil companies have recently been looking at hitherto unexplored deepwater environments for new sources of black gold. But along with a whole raft of complications and demands brought about by this new environment is the problem of how the oil can be transported safely and efficiently from the source. However, thanks to a breakthrough in marine rubber hose technology, Trelleborg’s Trelline system can now ensure the safety and efficiency of this connection, with significant overall cost reductions. 
In shallow fields, a metal pipe on the seabed is used to take the oil from Floating Production Storage and Offloading (FPSO) vessels to shuttle tankers moored at floating single-point mooring buoys about two kilometers away. But in deepwater oilfields, a metal pipe connection of this type laid on the seabed would be prohibitively expensive. “In the first deepwater field in Angola, Total, one of the world’s biggest oil companies, used a flexible steel pipe at about 300-500 meters below the surface,” explains Oil & Marine manager, Trelleborg Industrie. “But these pipes are extremely costly, which gave us the idea to develop Trelline, a flexible, reinforced rubber hose to provide this link instead,” he explains. Looking at the cost scenario, Trelline is an extremely competitive solution. “Its wider diameter requires less pumping pressure so the FPSO doesn’t need expensive booster pumps, saving up to USD 15 million,” says Cognard. “Engineers have also estimated even higher savings in terms of installation and maintenance costs,” he adds. Due to its specific design, Trelline hoses are almost corrosion- free and rubber also offers high thermal insulation, thereby lowering the oil’s viscosity – another factor in reducing pressure.

Furthermore, the Trelline solution comes in 12-meter sections, which can be replaced singly if necessary, rather than replacing the entire length of metal pipe. Trelline was developed and qualified in accordance with API 17K, a specification for rubber hose, in partnership with Single Buoy Moorings (SBM), the Monaco-based engineers who manufacture the floating buoys. SBM financed part of the qualification and engineering tests, and Trelleborg financed product development. The first order was received in September 2005, to supply a major oil company operating in West Africa and production  was completed in June 2006. Installation will be finished in October, and other projects are currently planned. The benefits of Trelline are many: “We have an enhanced brand image, we learned a  huge amount during the stringent FEA (finite element analysis) modeling and hose testing we had to do, and we have even developed Reeline, a new product based on similar technology for linking FPSOs to shuttle tankers in shallower water,” says Oil & Marine manager. “We’re very optimistic about Trelline’s success. It’s innovative but it’s based on proven technology. We’re being closely watched because, given the ease of installation and the potential savings, we will surely become the preferred solution,” he smiles.

QUICK FACTS

About Oil and Marine

Trelleborg has been present in the Oil & Gas industry for many years and offers a wide range of products, meeting most applications and needs. Our oil and gas hoses and assemblies are compliant with European and international standards.
QUICK FACTS

Trelline

Trelline is a reinforced bonded flexible hose made of rubber, steel ring reinforcement, integrated bending stiffener and steel armor cables reinforcement, end-fitted with a unique integrated gasket flange system.
The Trelline hose is available in submarine or floating configuration and meets the most stringent requirements of API 17K specification.
As of today Trelleborg has built over 1000 Trelline hoses and executed several API 17K certified projects all over the world.