Case Red Red WIne - Trelleborg Fluid Handling Solutions - Trelleborg AB

Red wine - VINITRELL hose

There are many factors at play when making wine. For its annual production of five million bottles, the wine cooperative USPDE in Saint-Emilion uses 1,500 meters of the Trelleborg wine hose Vinitrell.

The Union de Producteurs de Saint-Emilion (UDPSE) was the first ever wine cooperative in the Gironde – a département that includes the Bordeaux wine producing region and covers 120,000 hectares of vines. Only ten producers formed the cooperative back in 1932. Currently, it brings together 187 winegrowers with 800 hectares of vines, accounting for sales of EUR 27 M in 2008.

“We distribute some five million bottles of wine annually, 42 percent of which are exported,” says Bertrand Bourdil, Technical Director at UDPSE. “Unlike other cooperatives that sell wine wholesale to wine traders, we bottle all our production and are totally autonomous in terms of production and distribution.”
Sixty individual châteaux account for 60 percent of UDPSE’s business, with the remaining 40 percent comprising blended wines with the co-op’s own brands. “For us, the key is authenticity – we are continuing the great name of Saint-Emilion through fine wines that have a ‘handcrafted’ feel, despite our size,” Bourdil explains.

Indeed, since 2003, UDPSE has invested some EUR 8.5 M in a state-of-the-art winery with a capacity of two million liters that can receive up to 800 tons of grapes per day. “Our châteaux range from 0.35 hectare to about 20, but those producers know they can count on us to make the very best wine from their grapes with its own unique character,” says Bourdil.

Saint-Emilion wines are made from 80 percent Merlot, 15 percent Cabernet Franc and five percent Cabernet Sauvignon grapes, and the UDPSE team works very closely with producers throughout the year, awarding bonuses to those who best meet the quality standards established by the co-op. Careful checks on the vines are carried out to ensure the optimum date for the vendange, or wine harvest, which spells the end of the winegrower’s involvement. The quality of each batch is controlled on arrival, and the grower’s payment is instantly calculated, depending on quantity and quality.

The grapes are carefully transferred using gravity into stainless-steel vats, each containing 10,000-20,000 liters, where they macerate for up to four days. Yeasts are added and the temperature is raised to 20-22°C to trigger fermentation. This continues for about a week and the wine is subsequently macerated again for a fortnight before being pressed and racked off. It is then put into barrels in the dark cellar underneath the winery, which holds around 5,300 barrels. Some months later, the wines are fined where chemicals are used for clarification, removing all solids. They are then bottled the following spring.

The cooperative’s wines range in price from EUR 5 to EUR 28, and the bestseller is called Aurélius. “Aurélius was the co-op’s first branded wine, and it is a blend of wines from the eight communes that make up the appellation that we think truly represents a Saint-Emilion,” says Bourdil. Some 50,000 bottles of Aurélius are sold every year. “The key to a great wine is quality, which you get from treating wine with respect. We only use hoses from Trelleborg and have over 1,500 meters at present,” says Bourdil. The hoses are utilized wherever the wine needs to be transferred, such as from the vats to the barrels. “When we upgraded from the Citerdial to the Vinitrell hose, we were very happy, apart from the fact the hoses were red, which isn’t a color the winery team associates with hygiene. We asked Trelleborg to make us blue ones instead, which they did. We have always enjoyed a very good relationship with the company; one of mutual respect and cooperation – I’ll drink to that!”

FACT BOX

Winemaker's secrets revealed

Serge Uhart has been working as an oenologist, a wine scientist, at the Saint-Emilion cooperative since 2002.
We asked him what is needed to produce a great wine.
1. Firstly, you need good grapes.
There is no fine wine without fine raw materials, and they must be totally healty and perfectly mature.
2. You need a great team in the winery. When you are producing such large quantities as we do here, it is important that each wine maintains its own uique cahracter and expression of terroir So it is vital to have the right people for the job.
3. The equipment must be of the hightest quality - you need the technical means to ensure you are always working in the right conditions.
4. Scrupulous attention to hygiene is critical. Everything must be in tip-top conditions to ensure nothing is introduced that could spoil the wine.
5. A certain je ne sais quoi! We're making a product that brings happiness to people and it needs a touch of magic to create that special moment...

Related information