Water
• Total water consumption: 2.5 million (3.0) m3
The indicator has been changed to show total water consumption, which is more comprehensive. Historical comparison terms have been recalculated in the diagram below. The total volume of water by source is 47 percent from drinking water, 24 percent from private wells and 29 percent from surface water. Water is primarily used in production for cooling and washing. Major savings were made through various means, including recycling systems. Emissions to water are limited, but mainly comprise organic material.

Total water consumption includes both water in production and sanitary water, for example. Consumption decreased in both absolute and relative terms.
Measures to reduce water consumption comprise examples of installations for recycling fabrication water.