Environment
Trelleborg’s total environmental footprint has been reduced in almost every area, which is borne out by the changes in our relative environmental key ratios. The majority of the Group’s performance indicators showed a positive trend, a result supported by continued operational and resource-related efficiency enhancements.
Trelleborg’s goal is to reduce its direct and indirect carbon emissions by at least 15 percent, relative to sales, by the end of 2015 (“15 by 15”), calculated from the reference year of 2008.
Read more
Energy savings is a focus area for Trelleborg. All production plants shall have an energy-savings plan.
Read more
The principal raw materials are polymers and metal components, as well as additives including softening agents (oils), fillers, such as carbon black, and vulcanizing agents (sulfur, peroxides). Of the raw rubber used, approximately 38 (31) percent is natural rubber and 62 (69) percent is synthetic rubber.
Read more