Related Information






Connections

Straight ends

Straight ends for low pressure. A hose with straight ends can be connected in many ways. However, although cheap, this type of connections is only suitable for low pressures. One disadvantage is that when it is fitted in the pipe, it obstucts the flow through the hose. However, at low flow speeds, the turbulence caused by this is of secondary importance.


Low pressure collar


Reducing the diameter in a pipeline will cause turbulence and additional wear. For this reason we produce rubber reducers in any diameter and length. On spots on the inside of the reducer where the wear is the most present we can add more inner liner to lengthen the lifetime of the reducer.


Rubberflange with steel backingflange


This flange is used for medium pressures and suction hoses. The rubber flange means that the hose can remain relatively short, starting from a maximum angle of curvature. And because the wear layer rubber extends partly into the top edge of the flange, it forms a good seal with the flange connection itself.

Swivel flange

The swivel flange is used with medium service pressures at points where the bolt holes in the mounting flanges are not precisely aligned. The swivel flange simplifies fitting between 2 fixed points.

Double action flangeĀ®

Double action flangeĀ® for special applications. The double action flange is our most recent development. Its main advantage is that we van reduce the minimum pitch circle diameter by running the cord both along the bottom and the top of the flange ring. This creates more space underneath the flange ring to reduce the pitch circle diameter. This flange can be used in special situations where a short hose is needed with a high tensile strength and small pitch circle diameter. The form-fit flange construction guarantees maximum strength.

Steel couplings vulcanized

Our solid steel couplings are suitable for heavy and very heavy duty applications. They can be made with the smallest possible pitch circle diameters and are vulcanized into the hose. These couplings are also secured with our safety. We use these couplings as standard in our self floating hoses so that you can work during bad weather without the risk of a defective line.

Laminated flange

The laminated flange can be used in cercumstances where a relatively high compressive strength is required and where coupings vulcanized in cannot be used. To be used at service pressures of 10 bar and higher axial loads.

Latest updated 2008-04-18 |  Print this page Print this page |  E-mail this page E-mail this page
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message