Related Information






Design & Safety

Design

The basis of success is a flawless product. Our philosophy is as old as the company itself. It dates back to the beginning of the 50s and clearly states “We build the best rubber hoses for material transport using the latest state of the art technology and at a competitive price”. Design criteria are selected on this basis and have always gone hand-in-hand with practical development.

Today, our design department uses the most advanced simulation programming and design methods. The advantage of these is that the customer‘s specifications are “translated” in the best possible way into the product required. But they also mean that our know-how can be used on a wider scale in practice - which enhances the quality of our consultation work. As far as we are concerned, problems with dredger hoses do not exist. And if they do, we simply solve them.

Safety

A dredger hose from Trelleborg Velp is a reliable product all along the line. This reliability is guaranteed in a number of ways, starting with the concept. Because of their high level of wear resistance and flexibility, rubber material handling hoses are, by nature, ideal transport lines.

Hoses from Trelleborg Velp have proved to have a very long life in practice, even when pumping highly abrasive media. Overdimensioning is added to this excellent starting point in the design phase; we always make a dredger hose much thicker than specified. This safety margin is used to give the hose an additional shield against unforeseen circumstances. Other guarantees of safety and reliability are provided by our production control and test facilities. We can issue test reports for our products at the customer‘s request. But most of the tests which we carry out are intended for our own research. We also want to be sure at all times that we adequately satisfy all test and inspection requirements throughout the world.

 


Last updated 2008-04-18 |  Print this page Print this page |  E-mail this page E-mail this page
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message