Quality Statement
Trelleborg Velp aims at a high and constant level of quality. Therefore all production processes and procedures have been laid down in a Quality Assurance System set up in accordance with the guidelines of ISO 9001.
These guidelines are the lead in quality assurance, design, development, production, installation and after-sales. Trelleborg Velp is certified in accordance with ISO 9001 since Feb. 2002 For specific projects and on client's request, we make Quality Plans and Manufacturers Record Books in which all relevant information with regard to design, construction, production, testing, inspection and approval is gathered.
The Environmental Policy stipulates the direction and objectives of our environmental work at the same time that we clarify the tasks that lie ahead. The Environmental Policy constitutes the framework for the Trelleborg Group's activities that concentrate on the environment. According to the policy, Trelleborg Velp has developed an environmental policy as part of the ISO 14001 system. Since Feb. 2002 we have been certified in accordance with ISO 14001.