History

Trelleborg Automotive Kalmar AB has been the world leader in Rubber composite materials since 1988.



At the end of the nineteen seventies asbestos was prohibited as an ingredient in the formulation of friction materials. Asbestos was not only very functional in improving the performance characteristics of the materials e.g.: wear and friction, but it also assisted in absorbing noise and vibrations generated in parts of the braking system.
 
Since the prohibition of asbestos and it’s replacement in friction materials by other fibrous materials and metals, brake noise problems have increased to such an extent that studies show that it has become a major source of irritation to the vehicle driver. Solving of noise related problems is now of paramount importance to the vehicle manufacturers.
 
 
 
The company develops and manufactures noise damping shims, which when applied to the piston or finger side of a disc brake pad back plate provides an insulation. This barrier between the pad and the rest of the brake calliper absorbs vibrations and dampens any noise generated during vehicle braking. The shims are manufactured by the lamination of numerous combinations of rubber, steel, stainless steel, fibre glass and different adhesives.
 
The materials have unique characteristics, where the damping and isolating capacity of the rubber and adhesives is combined with the endurance of the metals against mechanical, thermal and chemical stress. A key feature of these shim materials is that, despite their complexity, they are thin, being around 0.6 to 1.2 mm.
 
Trelleborg Automotive Kalmar AB is today one of the worlds biggest shim producers, with their products installed in car and commercial vehicle brake systems around the Globe. The development of brake noise damping products has been very positive since 1988, with significant annual increases in turnover. History has shown that the requirement for noise damping solutions in automotive OEM, OES and After Market brake systems and lately in automotive and industrial applications increases annually.
Last updated 2011-03-30 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message