How can we help?

Americas Customer service
tel: (800) 344-0714


Europe, Africa, Oceania & Asia Customer service
tel: +39 0371 406321



Request information






Reduction of Make Ready Time

There can be various ways of reducing the make ready time of the press.



Correct paper release can reduce significantly the make ready time of the press, also for sheetfed application and for the new metal back blankets the elimination of calibrating paper can reduce the make ready time of a press by almost 20%. .  The underpacking offers a high resistance to the chemicals used in normal blanket washes etc, eliminating the risk of delamination, while there is no need to purchase and store separate underpacking.

Last updated 2011-06-20 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message





Featured blog

Newspapers get vote of confidence

If ever the newspaper industry heard some encouraging words, it was these: “Buffett, Be...

Featured whitepaper

As a PrintCity Partner we took part of various indepth industry resarch programes, see here below just a few of our findings. Webline is a quartely...

LinkedIn



uiqt|wBxzqv|qvoH|zmttmjwzo5kwuxzqv|qvoH|zmttmjwzo5kwu