New product effectively seals manholes

29 January 2010

Trelleborg Pipe Seals launches DRAIN FlexRib Manhole Seal that uses unique technology to give the most effective sealing without excavation.

 

Trelleborg Engineered Systems, through its Pipe Seals division, has introduced DRAIN FlexRib Manhole Seal, a chimney or collar seal designed to prevent infiltration and exfiltration from the top entry area of a manhole structure. Using patented Waveband technology the unit creates the most effective seal possible.

Prevents infiltration to and from manholes

“The top entry area is the part of the manhole that suffers most deterioration due to freeze thaw cycles at the surface, traffic loading, thermal expansion and contraction of the surrounding pavement, roads and other external forces. Prevention of infiltration to and from manholes is therefore a key factor in the effective sealing of pipe networks,” says Ian Ramsay, Sales Director for Trelleborg Pipe Seals Gateshead, UK.

 

DRAIN FlexRib Manhole Seal

 

“Our new DRAIN FlexRib Manhole Seal now offers a very quick to install and easy to use unit to achieve rehabilitation or restoration of pipe networks. Without the use of liquid resins, flexible materials and often extended cure times or pre-formed sections, which could possibly affect the future accessibility of manholes, manhole collars can now be completely sealed against extraneous flows in one simple operation.”

Patanted Waveband technology

The DRAIN FlexRib Manhole Seal is a spring seal system which utilizes a rubber seal in conjunction with an expanding stainless steel clip. Using patented Waveband technology the unit creates a more effective seal by concentrating the compressive force of the expansion band. The rubber is ‘captured’ between the band and the manhole structure.

 

Installation tool

Image shows installation tool

The seal is placed over the affected area and the spring clip is expanded using either a manual or hydraulically driven installation tool to press the rubber seal into position over the damaged area. Installing the seal creates a watertight seal between the manhole frame casting and top of the manhole cone. The design of the seal allows it to move vertically and/or laterally whilst maintaining a watertight seal.

The seal itself is made from a premium quality rubber compound and is available in four widths, along with a FlexRib extension seal, to cover all types of manholes.



For more information, please go to: 


Press Service:

This press release is available for download in English. If you reproduce information from this release please give contact details as:
www.trelleborg.com
E-mail:  

 English [doc]
 
Click here to request high resolution images.

Last updated 2010-05-27 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message





© Trelleborg AB (publ), P.O. Box 153, SE-231 22 Trelleborg, tel: +46 410 670 00
Site policy   |   Site map
uiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwuuiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwu