Trelleborg suspension components for Korea's new high-speed train


Rotem of Korea has chosen anti-vibration components from Trelleborg Industrial AVS (TIAVS) for the primary suspension of KTX-II, its new high-speed train which is due to roll out on the Honam-Jeolla line during 2010


Trelleborg is supplying Metalastik® half-shell bearings™ for the anti-roll bar system which is designed to limit the movement of the train body as it negotiates the track's curves.

Metalastik® half-shell bearings™



The bushes are mounted in pairs at either end of each anti-roll bar and are designed to provide progressive spring stiffness and maximum flexibility under full load conditions.

Rotem's KTX-II is a unique design using all-Korean technology and is based on the earlier Korean Train eXpress KTX-I, which ultimately derived from the TGV.  Although designed to run at speeds up to 330 kmh, KTX-II is capable of 350 kmh and is expected to reach a maximum speed of 400 kmh by 2012, making it by far the fastest of all the commercialized high speed trains.  The protoype is due to begin its test programme in 2008.

Rotem has already won the contract for trains on the Honam-Jeolla line, which is due to open in 2009 but the KTX-II will also run on a number of other new lines which are being planned by Korea.  In addition, Rotem has received expresions of interest from the USA, Turkey and Brazil.

Rotem is part of the Hyundai Motor Group and, in addition to light rail vehicles, its Changwan-based rail division designs and manufactures electric and diesel locomotives, Maglev and high-speed trains, suburban train units, passenger and freight wagons.

Trelleborg Industrial AVS is a world leader in the design and manufacture of rubber to metal bonded components for anti-vibration applications and suspension systems. 
There are three main brands: Metalastik® is used in rail and marine applications, TrellExtreme® in agriculture/off-highway and Novibra® in industrial and power generation applications.
 
The company’s head office, technical centre and research and development units are located in Leicester, UK while production is divided between Leicester, Sweden, India and China.

Trelleborg Industrial AVS is approved to ISO 9001:2000.
 
For more information on Trelleborg Engineered Systems, Trelleborg AVS:

Press Service:

This press release is available for download in English. If you reproduce information from this release could you please give contact details as:
www.trelleborg.com
Email:  

English [doc]

Click here to request high resolution images.

This article relates to the following industries:

  • Transport
 
Last updated 2008-09-05 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message





© Trelleborg AB (publ), P.O. Box 153, SE-231 22 Trelleborg, tel: +46 410 670 00
Site policy   |   Site map
uiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwuuiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwu