Syntactic foam adds strength and buoyancy

From drinking cups to the space shuttle, syntactic foam is used in a multitude of applications.


Meaning “to piece together,” the word “syntactic” is derived from the word “syntax.” Fitting this definition, syntactic foam consists of hollow glass spheres known as microballoons that are joined together in a binder phase, usually in a polymeric resin system. As Trelleborg Emerson & Cuming’s syntactic foam uses a rigid glass wall as a void former, it is much stronger than traditional “blown” foam with its unreinforced air void. It is used as a structural reinforcement as well as a buoyancy agent, insulator, and thermoforming material. The diameter of the hollow spheres can range from a couple of inches down to the thickness of a single strand of human hair.

Syntatic Foam

Offshore applications
Trelleborg uses syntactic foam extensively in offshore applications. Some of the more common applications are used as buoyancy material for use in undersea exploration and drilling operations.

“When you make a vehicle for the deep ocean, it needs to be neutrally buoyant so that it doesn’t rise or sink,” explains Trelleborg Emerson & Cuming Vice President of Technology, Dr Gary Gladysz. “Syntactic foam counterbalances the heavy construction of the vehicle.”

Used to reinforce hollow areas
Aircraft manufacturers that include Airbus and Boeing reinforce hollow areas within the aircraft with syntactic foam. Special formulations of syntactic foam are used by NASA to insulate the fuel tanks and solid rocket boosters of the Space Shuttle.

The automotive industry is also beginning to take notice of syntactic foam’s potential. “As automotive manufacturers continue to seek new and innovative ways of reducing weight and, consequently, improving fuel economy, while at the same time enhancing such safety features as crash absorption, syntactic foam is opening new opportunities for the industry,” says Gladysz.

In the production of disposable drinking cups and plastic packaging, syntactic foam is used because it is a highly durable material capable of withstanding the millions of cycles associated with repetitive thermoforming.

New functionality
At the heart of syntactic foam are glass microspheres. In addition to producing various types of syntactic foams, Trelleborg Emerson & Cuming produces both high-performance glass microspheres and, in a separate process, coated microspheres which are used in many different industries. “Coating the microspheres adds new levels of functionality such as dielectric or thermal imaging properties,” says Gladysz. “When these coated microspheres are used in the production of syntactic foams, you effectively introduce additional functionality. This opens the door to exciting new opportunities.”


For more information on Trelleborg Engineered Systems, Trelleborg AEM:

Press Service:
This press release is available for download in English and other languages. If you reproduce information from this release could you please give contact details as:
www.trelleborg.com
Email:  

English [doc] 
French [doc]
German [doc]
Italian [doc]
Spanish [doc]
Swedish [doc]

Click here to request high resolution images.

This article relates to the following industries:
  • Aerospace
  • Automotive
  • Construction
  • Food and beverage
  • Marine
  • Oil and gas
  • More solutions
Last updated 2008-09-29 |  Print this page Print this page |  E-mail this page E-mail this page
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message





uiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwuuiqt|wBvm%w{H|zmttmjwzo5kwuvm%w{H|zmttmjwzo5kwu