Contact Us
Trelleborg Emerson & Cuming, Inc.
290 Forbes Boulevard
Mansfield, MA 02048-1817
USA
Tel: +1 774 719 1400
Fax: +1 774 719 1410







Syntactic Foam Buoyancy Materials

Syntactic Foam Buoyancy Materials
Alvin, the vehicle used in the discovery of the Titanic was constructed using Trelleborg's man rated syntactic foam buoyancy materials...
Trelleborg Emerson & Cuming, Inc manufactures several different classes of syntactic foam for undersea buoyancy applications. Blocks of the foam are typically cast in 0.5 and 1.0 cubic foot sizes, which then are used to prepare large buoyancy modules that can be readily shaped to conform to hull contours and outfitted for installation in the forward and aft free-flood areas of submarines.
 
Oceanographers also depend on syntactic foams to suspend instrumentation in deep ocean studies. For these applications, the syntactic foam is used in either block form or custom molded shapes for installation in manned and unmanned submersibles such as the famed Alvin and Jason vehicles that were used to discover and explore the Titanic.
 
 
Last updated 2007-09-04 |  Print this page Print this page |  E-mail this page E-mail this page
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message




uiqt|wBmumz{wvH|zmttmjwzo5kwumumz{wvH|zmttmjwzo5kwu