Related Information
Contacts






Active Force Cancellation

A quiet ride
 
An innovative noise reduction system that uses active force cancellation sparks considerable interest among the world’s major automobile manufacturers.

In the past, attempts to reduce the effects of noise and vibration in vehicles have been based on passive technology and the use of elastomeric springs for isolation. However, Trelleborg’s anti-vibration experts have now developed  an innovative noise reduction system that uses active force cancellation, sparking considerable interest among the world’s major automobile manufacturers.

The active force cancellation system uses special actuators located near mount attachment points to generate waves at the same frequency and amplitude as those created by noise and vibrations. When transmitted completely out of phase, the waves cancel each other out.


When two sound waves meet while traveling along the same medium and are completely out of phase, the amplitude or height of the waves cancel each other out.

“It sounds simple, but we have been working on it for more than a decade,” smiles AFCManfred Hofmann, technical director at Trelleborg Automotive’s Technical Center in Höhr-Grenzhausen, Germany. Now Trelleborg is talking to automotive manufacturers and offering the active force cancellation system as an alternative to the current use of balance shafts for noise reduction. “Use of balance shafts is quite expensive technology and it mainly works for higher RPMs, so we’re suggesting manufacturers opt for an active system instead, which offers wider performance,” says Manfred Hofmann.

The system is also perfectly suited to new and more environmentally-friendly engine configurations, explains Manfred Hofmann.

“Manufacturers are looking to reduce emissions by introducing new engine configurations that switch off certain cylinders when the engine is not operating at maximum power. Although this contributes to fuel economy, it creates more vibration and noise that our technology can reduce.”

Trelleborg is also looking to target specific vehicles with particular noise reduction requirements. “Some vehicles, such as three-cylinder diesels, have greater need for such technology,” says Manfred Hofmann. “Rather than being fitted as standard, active force cancellation systems could be ideal for those cars whose engines create more vibration than others,” he explains.

Another potential use for the technology was highlighted by recent inquiries from one major manufacturer who is currently examining a project to create the perfect engine sound to suit the car model. “Rather than canceling it out, they want to tune the sound to create a desirable sound quality with specific harmonics,” says Manfred Hofmann.

For the cars of the future, there is still a role for active force cancellation to play, contends Manfred Hofmann.

“With the industry looking to fuel-cell technology in the future, engines will make a lot less noise once the internal combustion is removed. However, there could still be problems with wind or other disturbing noises, which would be an ideal application for us to create a better driving experience.”
 
For more information please contact:
Enrico Kruse
Advanced Engineering Manager
Tel: +49 2624 12 233
Fax: +49 2624 12 146
Email:

 
Last updated 2009-09-11 |  Print this page Print this page |  E-mail this page E-mail this page   Facebook   Twitter
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message





uiqt|wBmvzqkw5sz}{mH|zmttmjwzo5kwumvzqkw5sz}{mH|zmttmjwzo5kwu