Electronic Screen Printing

Unitex has been supplying squeegees into the Screen Printed Electronic and Industrial market sectors for over 20 years. Our Blue Chip customers recognise the excellent advantages of accuracy and repeatability of the Unitex product. They refuse to save a few dollars on the price of a squeegee and potentially jeopardise a print run worth many thousands of dollars.



Electronic Scrren Printing

Markets and Applications (Some of our many uses)
  • PDP – Plasma Display Panels
  • PCB – Printed Circuit Boards
  • RFID – Radio Frequency Identification
  • Thin film transistor circuits 
  • Displays
  • Bio-Medical Devices
  • Capacitors
  • Fuel and Solar Cells

The Electronics Squeegee:
ULON HP is at the forefront of the high value screen printed electronics sector. It is chosen for:
  • Consistent print thickness, ideal for fine tracks and spacing
  • Consistent quality batch to batch, squeegee to squeegee
  • Bespoke parts for many applications
  • Resistance to abrasion
  • Cost effective

Performance
Because Unitex manufactures its squeegee to +/- 2.5° Shore A (Durometer) the screen printer is ensured they can fit the a replacement Unitex squeegee and it will perform as effectively the previous one. This reduces set up times and ensures the printing is in specification and right first time. 
 
Quality
Unitex adheres strongly to their ISO 9001 accreditation. We have complete traceability from raw materials, thorough manufacturing and the finished product. Unitex has vastly experienced Quality and Inspection departments. We inspect out any potential defects unlike some of our competitors who just ship and let the user do it. We also test every single sheet of material we manufacture, a claim some others cannot match.
 
RoHS
Most squeegees use heavy metals as a catalyst in the manufacturing process. ULON HP does not. While the squeegee does not go into the finished product more and more of our clients are asking for our RoHS certification as this is the last piece in a fully environmental manufacturing process. 
 
Printing edge
Our squeegees are machined using state of the art CNC equipment. The printing edge is consistently sharp and is capable of depositing inks or pastes down to 10 µm (Microns). Some squeegee manufacturers make a Moulded squeegee but the radius at the printing edge makes it difficult to deposit the fine lines required. Also with the moulded product as soon as the edge is dressed it looses its ‘moulded’ properties.
 
Partnership

Unitex works closely with partners, both new and existing, to develop new printing and production techniques. You will have access to our technical team who are focused on offering service and advice. We will supply Free of Charge samples to help you set up your production and manufacturing process.

 

ISO 14001ISO 9001

 

 

 


 
For further information, please contact:

 

Last updated 2008-03-24 |  Print this page Print this page |  E-mail this page E-mail this page
E-mail this pagex


Receiver e-mail address


Your e-mail address


Subject


Your message




uiqt|wBxi}t5pijjmznqmtlH|zmttmjwzo5kwuxi}t5pijjmznqmtlH|zmttmjwzo5kwu