Trelleborg tires chosen again by the World’s Strongest Man Competition

Trelleborg_world-strongest-man-for-WSM_final

Trelleborg tires chosen again by the World’s Strongest Man Competition

In 2014, Trelleborg TM600’s were once again the tire of choice for the World’s Strongest Man competition.  The event was staged at the Commerce Casino in Los Angeles, California. 

Trelleborg TM600's were used in the "Super Yoke" event. Two competitors at a time, attempted to carry two 520/85R38 TM600 tires and the yoke down a 30 yard (approximately 25 meters) track. Ten athletes raced against the clock with the winner of the event having the fastest time. The combined weight carried by each competitor was 1,000 lbs (453 kg).

Andrea Masella, Marketing Manager at Trelleborg Wheel Systems for North America, says: “As the athletes are committed to excellence performance, so is Trelleborg. From development to manufacturing and then delivery, Trelleborg strives to go beyond the standards, just like the World’s Strongest Man.”

To see who won the competition in the U.S., tune into the CBS Sports Network in June. The current schedule shows first competition will be aired on June 4 and continuing through to June 15.

Download the entire document of the press release

"Trelleborg tires chosen again by the World’s Strongest Man Competition"

For more info regarding our press releases, go to:

www.trelleborg.com/wheelsystems/pressroom

More images regarding the World's Strongest Man competition are available on

www.flickr.com/TrelleborgAgri